MOVE.RUNSPEED

Description

Sets the maximum speed allowed during an incremental (MOVE.GOREL) or absolute (MOVE.GOABS) move, and sets the commanded speed during a velocity move (MOVE.GOVEL). Specify MOVE.RUNSPEED before initiating any move commands.


  • MOVE.RUNSPEED must be a positive value.

  • MOVE parameters are only valid when DRV.OPMODE = 2 and DRV.CMDSOURCE = 5.

General Information

Type

R/W

Units

Depends on UNIT.VROTARY or UNIT.VLINEARUNIT.ACCLINEAR

Rotary: rpm, rps, deg/s, (Custom Units)/s, rad/s

Linear: counts/s, mm/s, µm/s, (Custom Units)/s

Range

N/A

Default Value

N/A

Data Type

Float

Variants Supported

This parameter is only supported on AKD BASIC drives.

Fieldbus Information

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

1138

Yes 64 bit No

M_01-05-11-000

Related Topics

MOVE.GOVEL | MOVE.GOREL